Solution
Smartwatch Milling
Smartwatch milling is a precise manufacturing process where machines meticulously form parts of the smartwatch into a desired shape.

Smartwatch milling is a precise manufacturing process where machines meticulously form parts of the smartwatch into a desired shape. In order to maintain precision and quality, forces of the milling machine must be monitored and controlled to produce consistent smartwatch components.
Interface’s 6AXX 6-Axis Load Cell can be installed into the milling machine. As the machine cuts and create smartwatch components, the multi-axis load cell collects data on six axes (Fx, Fʏ, Fz, Mx, Mʏ, Mz). When connected to the BX8-HD44 Data Acquisition, Data can be logged, graphed, and displayed when connected to a computer with supplied BlueDAQ software.
Interface’s 6AXX 6-Axis Load Cell could measured and monitored all forces and torques (Fx, Fʏ, Fz, Mx, Mʏ, Mz) of the milling machine as it creates smartwatch components. The machine produces consistent and controlled smartwatch components.