Solution
Bolt Tension Monitoring
A customer wants to monitor the tension of the bolts that are used on their industrial large metal pipes.

A customer wants to monitor the tension of the bolts that are used on their industrial large metal pipes.
Interface suggests installing multiple LWCF Clamping Force Load Cells, each connected to WTS-AM-1E Wireless Strain Bridge Transmitter Modules. The load cells are installed under the tightened bolts on the pipes. The load cells will measure the compression forces from the bolts, and the real-time results are transmitted wirelessly from the WTS-AM-1E’s to the WTS-BS-6 Wireless Telemetry Dongle Base Station when connected to the customer’s PC. Real-time results from the LWCF’s are displayed using provided Log100 Software.
Interface’s load cell monitoring system successfully monitors the compression forces of the bolts in real time.