Solution
Bike Helmet Impact Test
A bike manufacturing company wants to test the impact of a bike helmet when dropped from different heights, onto a flat surface such as an anvil.

A bike manufacturing company wants to test the impact of a bike helmet when dropped from different heights, onto a flat surface such as an anvil.
Interface suggests installing one of their 1101 Compression-Only Ultra Precision LowProfile™ Load Cell at the bottom of an anvil. The bike helmet is then dropped from multiple heights, at multiple angles, onto the anvil. The measurements from impact are then recorded and logged when attached to the customer’s PC laptop or computer.
Interface’s 1101 Compression-Only Ultra Precision LowProfile™ Load Cell measured accurate force results of the bike helmet impacts at different height levels.