Custom OEM Solutions


Turning an active component into a sensor means that we can include a transducer in-line in a system and both track data
and perform actions based on the data. As an example, an automated manufacturing line could include a force sensor
on several different machines to track certain data, such as pressing force or torque. Having this sensor included in the
manufacturing line allows the users to track performance or simply track the normal data so when abnormalities occur,
they can determine whether a machine needs a repair or replacement. The active part of the systems means that the
component can act autonomously when the data tells it to, rather than needing human intervention.