Livestock Weighing System
Interface’s solution is to bolt four SSB Sealed Beam Load Cells at the bottom of a metal platform, that is placed on the inside of the customer’s cattle cage. Once the cow has walked onto the plate, the SSB Sealed Beam Load Cells will measure the force pressure applied. With all four connected to JB104SS Junction Box, which is then connected to the 480 Bidirectional Weight Indicator, combined accurate weight results will be displayed.