7 search results for:

IQ Blog

Force Measurement is Fundamental in Material Testing

Interface load cells, multi-axis sensors, and data acquisition systems are used for material testing. Common uses of force measurement in material tests include applications to measure hardness, torsion, strength, compression, bending, shear, impact, creep, fatigue, and nondestructive capabilities. It is common to have our 1200 LowProfile load cells installed into material testing machines at test labs and onsite. We also supply a variety of miniature load cells and load pins for material testing, depending on the type of equipment and environment used for tests.

IQ Blog

Demystifying Specifications Webinar Recap

Interface's Demystifying Specifications recorded webinar details product specification basics, key values, terms to know, how to read a datasheet, what specs matter most in force measurement, and commonly asked questions. For Interface, specifications are detailed descriptions that outline the characteristics, features, and qualities of our products, systems, or services. Throughout the webinar, Interface experts provide tips on what to consider for high-speed, durability, precision and speciality load cell, torque transducer, multi-axis sensor and instrumentation product requirements.

IQ Blog

Why Is Load Cell Zero Balance Important to Accuracy?

Load cell zero balance is the signal of the load cell in the no-load condition. It is defined as the output signal of the load cell with rated excitation and no load applied. It refers to the amount of deviation in output between true zero and an actual load cell with zero load. It is usually expressed in the percentage of rated output (%RO). Zero balance is a test that can be done to understand calibration on a load cell.

IQ Blog

Load Cell Basics Webinar Recap

Interface applications and load cell expert Keith Skidmore was the featured presenter at the latest ForceLeaders Forum hosted event, Load Cell Basics. In his comprehensive presentation, he highlights key subjects including fundamentals of load cell design, sensor specifications, use cases, troubleshooting and valuable performance related topics.

IQ Blog

Load Cell Basics Technical Q&A Part One

Interface Technical Q&A for Load Cell Basics Part One answers questions about strain gages, creep, temperature compensation, capacity testing, pressure, TEDS and more.

IQ Blog

Specifying Accuracy Requirements When Selecting Load Cells

Interface load cells have detailed specification datasheets that outline accuracy and performance factors by model and capacity including nonlinearity, hysteresis, nonrepeatability, static error band and more.