Solution
Mouse Touch-Pad Force Testing
A laptop manufacturer wants to ensure the functionality of their mouse touch-pads.
A waste management company wants to measure the capacity of their waste containers in order to know when it is time to dispose the waste. A wireless system is also preferred to record the force results.
Interface suggests using the SMTM Micro S-Type Load Cell, from their Interface Mini™ line. The SMTM can be installed in the customer’s actuator test rig. The SMTM will record the amount of force it takes to press on the track-pad and create a response, on different areas of the track-pad. The actuator will aid with tactile feedback by providing movements such as dragging or creating friction. The measurements can be captured using the 9330 Battery Powered High Speed Data Logging Indicator through an SD card, or another laptop directly.
The SMTM Micro S-Type Load Cell was able to measure the forces applied to the mouse touch-pad at different locations. Interface’s products successfully measured the forces needed to make the mouse touch-pad create a response.