Facebook Twitter LinkedIn YouTube
toll-free: (800) 947-5598

Industries Aerospace

F/A-18 Fighter Aircraft Wing Fatigue Testing

Wing Fatigue Testing
Close-up: Single Cylinder with Indicator
IAGB Test Set-up

Before any of the U.S. Navy’s F/A-18 twin-engine supersonic fighter jets can be put into operation, the wings of the aircraft must undergo fatigue testing in a controlled environment to ensure that they are capable of withstanding the forces that will be encountered during real-world flight throughout the lifetime of the aircraft. Highly accurate measurements must be recorded in order to make sure that a near-exact replication of in-flight conditions is being achieved.

Learn how this is accomplished using the Interface Model 1248 Precision Flange LowProfile™ Load Cell and an indicator.

Download the Application Note below.

 Wing Fatigue Testing App Note.pdf