Facebook Twitter LinkedIn YouTube
toll-free: (800) 947-5598

Industries More Applications

Hydrofoil Testing in a Wave Tank

Hydrofoil design is a delicate balance between performance and complexity. Finding the right shape without using overly complex angles to achieve the desired amount of lift is crucial when designing a successful hydrofoil. Once an engineer’s concepts are ready for testing, using the best force measurement equipment is required to sense the subtle differences between hydrofoil designs.

Learn how this was done using an Interface Model 3A120 3-Axis Load Cell along with a Model BSC4D Multi-Channel Bridge Amplifier & PC Interface Module.

Download the Application Note below.

 Hydrofoil Testing in Wave Tank App Note.pdf