Need It Fast
Home Company Certifications


A2LA Accreditation
ISO 17025 Accreditation

A2LA Accreditation

Interface is A2LA Accredited for Torque and Force Calibration

Interface calibration certificates are the most complete in the industry. Certificate information includes tabulated measurement variables data, zero balance, bridge input/output resistance, computed nonlinearity and hysteresis, and traceability statements.

Both force and torque calibration are A2LA Accredited at Interface per ISO/IEC 17025. An accredited certification is offered at a nominal charge.

A2LA Accreditation

A2LA has accredited INTERFACE, INC. Scottsdale, AZ for technical competence in the field of Calibration.

This laboratory is accredited in accordance with the recognized International Standard ISO/IEC 17025:2005 General Requirements for the Competence of Testing and Calibration Laboratories. This laboratory also meets the requirements of ANSI/NCSL Z540-1-1994 and any additional program requirements in the field of calibration. This accreditation demonstrates technical competence for a defined scope and the operation of a laboratory quality management system (refer to joint ISO-ILAC-IAF Communiqué dated 8 January 2009). Presented this 21st day of September 2010.

 A2LA Scope of Accreditation